Problems with the example KeyboardHost

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problems with the example KeyboardHost

1,602件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by paulo on Thu Aug 30 12:56:24 MST 2012
Hi.

I'm testing the examples Example_KeyboardHost and Example_VirtualSerial on a plate LPCXPRESSO baseboard along with the link containing the micro LPC LPC 1769.
When I run the project Example_KeyboardHost without connecting a USB cable to connector X3 containing a FT232RL connected to UART3 the program runs normally but when I connect the cable occurs the errors identified in the images below, it all before I connect the keyboard. If I run the program with the cable already connected it runs normally, but when I open a terminal application and point to that door he gives the same mistakes of the images below.
In case the project Example_VirtualSerial it works normally, but I just connect the USB cable to the connector X3 to encounter the same problems.
In the case of the example he uses Example_KeyboardHost UART3 to send keystrokes via the keyboard, but as I said earlier, I just connect the cable to the problem below occurs.
Anyone have any tips for me?

ラベル(1)
  • USB

0 件の賞賛
返信
1 返信

1,594件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nxpUSBlib team on Wed Sep 19 16:38:32 MST 2012
Check the owners manual to make sure your jumpers are set correctly. That X3 connector doubles as a firmware upgrade port for Flashmagic and some of the signals are connected to reset based on the jumper settings by default.
0 件の賞賛
返信