Problems with the driver of the example VirtualSerial

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problems with the driver of the example VirtualSerial

1,635 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by paulo on Wed Jul 11 04:57:32 MST 2012
Hi,

I am testing the sample VirtualSerial with microcontroller LPC1769 and the board LPCXpresso base board. My computer is windows 7, 64 bits and when I connect the USB cable it recognizes the device nxpUSBlib CDC Demo in section other devices, but can not find the driver for it and therefore it does not work.

Anyone know of any driver I need to install on my computer to run this example?

Thanks for any help or hint.

Paulo
Labels (1)
0 Kudos
Reply
2 Replies

1,619 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by paulo on Wed Jul 11 11:01:33 MST 2012
Thanks TKoe, problem solved.

Regards,
Paulo

0 Kudos
Reply

1,619 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TKoe on Wed Jul 11 06:56:30 MST 2012
Hi,

there is a .inf file in the directory of that example. When Windows is asking you to find a driver select this file. I could only test this on XP, but it should work with 7, too.

Regards,
Tim
0 Kudos
Reply