Problems with the debugger

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problems with the debugger

1,087 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by john_doe on Tue Sep 09 07:48:34 MST 2014
I want to debug my programm with the debugger on lpcxpresso. A few hours ago it was still possible.
When I now start the dubugger there is the following text in the console:

The target endianness is set automatically (currently little endian)
/home/build/work/GCC-4-8-build/src/gdb/gdb/linespec.c:2445: internal-error: decode_line_full: Assertion `state->canonical_names.suffix != NULL' failed.
A problem internal to GDB has been detected,
further debugging may prove unreliable.
Quit this debugging session? (y or n) [answered Y; input not from terminal]
/home/build/work/GCC-4-8-build/src/gdb/gdb/linespec.c:2445: internal-error: decode_line_full: Assertion `state->canonical_names.suffix != NULL' failed.
A problem internal to GDB has been detected,
further debugging may prove unreliable.
Create a core file of GDB?
This application has requested the Runtime to terminate it in an unusual way.
Please contact the application's support team for more information.
(y or n) [answered Y; input not from terminal]

What did I do wrong?
I use a LPC4088.
Labels (1)
0 Kudos
Reply
1 Reply

1,046 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Tue Sep 09 08:08:28 MST 2014
Breakpoints?

http://www.lpcware.com/content/forum/issues-lpcexpresso-70092
0 Kudos
Reply