Problem with programming LPC1768 by JLINK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problem with programming LPC1768 by JLINK

1,202 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rebo on Tue Jun 25 00:40:07 MST 2013

Hi


Please Help...


I have a LPC1768 soldered on my PCB. For the first time, when the device was blank, it was programmed correctly. After that, JLINK cannot connect and program flash.


The error is as below:


Could not power up debug port: Control/Status register reads 00000F03


Failed to connect


 


I use "J-FLASH ARM V4.34a".


The external clock frequency is 8MHz.


The PLL setting is : M=150 , N=8

标签 (1)
0 项奖励
回复
0 回复数