Problem with float variable

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem with float variable

6,091 Views
Nadia
Contributor III

Hello everyone, I have a problem with floating point variables. I am defining a variable as float, to which I add a constant, with a value of 54.3. The value is stored in the variable as 54.2999999, this happens because of a hexadecimal conversion issue, but how can I avoid it? Where can I set the variables somehow ?

Thank you very much.

0 Kudos
Reply
10 Replies

6,088 Views
frank_m
Senior Contributor III

I t would be best to show the related code here.

However ...

> I am defining a variable as float, to which I add a constant, with a value of 54.3.

This number is not a float, but a double. To avoid C type promotion issues, be more specific with constants. In your case, it would be 54.3f. Otherwise, a double constant is created by the compiler, and then rounded / converted to float.

And second, float has a quite limited accuracy, consisting of only 24 bit mantissa.

0 Kudos
Reply

6,086 Views
Nadia
Contributor III

@frank_m OK, but can my problem be solved?

0 Kudos
Reply

6,082 Views
frank_m
Senior Contributor III

But what is your problem ?

The float format has a limited amount of numbers it can express exactly, and thus a limited accuracy. But  does it affect the correctness of your code, or the stability of algorithms you are using ?

If you get hung up about the deviation in the smallest digit, I cannot help you.

0 Kudos
Reply

6,078 Views
Nadia
Contributor III

@frank_m My problem is as follows:
I create a variable type float, and I save a value in it, specifically I save the constant 54.3. With this variable I work, and the problem is that when I save it as float it becomes the value 54.299999, and I would like to know if this can be defined in some configuration and that the value saved in this variable does not change to 54.29999 and stays at 54.3.

 

I hope I have explained myself well.
Thank you very much.

0 Kudos
Reply

6,075 Views
frank_m
Senior Contributor III

You write the constant "54.3" in your code - what is actually stored (and how) is a different matter.

> ...and the problem is that when I save it as float it becomes the value 54.299999

I suspect with "becoming the value 54.299999" you mean printing out as double number, probably using printf().

Not sure if you are aware, but the POSIX / standard library function printf() only knows of double arguments, and will convert floats accordingly. For the clib variants coming with MCUXpresso, you would need to check the manual, what printf and similar functions actually implement.

However, reducing the precision (e.g. with "%.1f" instead of "%f") will give you a rounded result, i.e. "54.3" instead of "54.299999" in your case.

Example:

float  fn = 54.3f;

printf "float number = %.1f ", fn);

0 Kudos
Reply

6,070 Views
converse
Senior Contributor V

54.3 cannot be represented exactly, using float (or double, for that matter) and 54.299999 is as close as you can get. There is nothing wrong, it is a fundamental limitation of using binary to represent floating point numbers - you can only ever get a (close) approximation.

0 Kudos
Reply

6,068 Views
converse
Senior Contributor V

p.s. This article is a good basic explanation of why you cannot represent 54.3 exactly, using float or double.

https://www.cs.yale.edu/homes/aspnes/pinewiki/C(2f)FloatingPoint.html

 

0 Kudos
Reply

6,053 Views
Nadia
Contributor III

@converse 

Thank you very much.

I know that it can't be represented as 54.3 because it works in binary, but I wanted to know if there was a way to configure the variables to save the exact number.

Thank you very much again.
Best regards.

0 Kudos
Reply

5,989 Views
Ray_V
Contributor V

it all depends on what you are trying to do.

You can always save and use as a double keeping in mind that when you print you need to round to 1 decimal place.

Another option is to save it in 0.1 units, for example, you can save it as integer 543 keeping in mind that this means 543 x 0.1

We can't say what is the best way to do it because we don't know what you are trying to achieve

0 Kudos
Reply

6,050 Views
converse
Senior Contributor V

You cannot store 54.3 exactly, in binary (I.e. a variable). You could store it is a string.

0 Kudos
Reply