Problem with debugging using LPC 2138 with J-Link

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem with debugging using LPC 2138 with J-Link

2,218件の閲覧回数
akshaychacko
Contributor I
I am trying to debug my LPC 2138 processor using Keil uVision. However, I don't seem to be able to step into the actual code using my J-link. It shows the disassembly but never enters the actual code when I try to debug. I called Keil support, and he guided me through examples where we saw that it does not enter the code in any instance The support at Keil suspected that the processor is stuck on its pre-programming routine and never actually getting into the code to execute He thought there may be some NXP specific code that can't be erased and therefore is not allowing a proper debug If I try to set a breakpoint, I am still not able to enter the code. It just says undefined line number to my breakpoint regardless of where I put it and then the code only loops through the disassembly without ever stepping through the code, starting at address 0x00000000. I am able to get one blinky example to debug, but nothing else. It is worth noting that I am unable to erase all of the flash memory using a program like FlashMagic. How can I step through my code?
ラベル(1)
タグ(4)
0 件の賞賛
返信
2 返答(返信)

2,092件の閲覧回数
converse
Senior Contributor V

Given your description - especially that FlashMagic cannot erase the whole device - it suggests a power problem. So, make sure you have enough power being supplied to the board,

0 件の賞賛
返信

2,092件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Akshay,

Unfortunately, I have not the LPC2138 board, which is very old. I attach two screenshot which tell you how to configure the J-link setting based on LPC54114 board.

After you success to compile/link, you can click Debug->Start/Stop Debug Session to download code as the second screenshot.

Hope it can help you

BR

Xiangjun rong

pastedImage_2.png

pastedImage_1.png

0 件の賞賛
返信