Problem with SPI SCLK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem with SPI SCLK

2,593件の閲覧回数
smbov
Contributor I

Hi!,

Firstly, I want to say hellow to everyone because it is my first question in this forum. Thank you to everyone.

I want to use a SPI connection with the LPC824 but the problem is that although CPOL and CPHA are set to 0, the SCLK starts at low state but then, before y send a byte, it mantains a high state. 

I let you the SPI startup code below:

///spi
Init_SPI_PinMux();

Chip_GPIO_Init(LPC_GPIO_PORT);
Chip_GPIO_SetPinDIROutput(LPC_GPIO_PORT,0,PIN_psel);
Chip_GPIO_SetPinDIRInput(LPC_GPIO_PORT,0,PIN_busy);
Chip_GPIO_SetPinDIRInput(LPC_GPIO_PORT,0,PIN_irq);
Chip_GPIO_SetPinState(LPC_GPIO_PORT,0,PIN_psel,true);


Chip_SPI_Init(LPC_SPI1);
Chip_SPI_ConfigureSPI(LPC_SPI1, SPI_MODE_MASTER | /* Enable master/Slave mode */
SPI_CLOCK_CPHA0_CPOL0 | /* Set Clock polarity to 0 */
SPI_CFG_MSB_FIRST_EN |/* Enable MSB first option */
SPI_CFG_SPOL_LO); /* Chipselect is active low */

Chip_SPI_Enable(LPC_SPI1);
Chip_SPI_ClearStatus(LPC_SPI1, SPI_STAT_CLR_RXOV | SPI_STAT_CLR_TXUR | SPI_STAT_CLR_SSA | SPI_STAT_CLR_SSD);
Chip_SPI_SetControlInfo(LPC_SPI1, 8, SPI_TXCTL_ASSERT_SSEL | SPI_TXCTL_EOF | SPI_TXCTL_RXIGNORE);
LPC_SPI1->DIV=0;

Thank you

ラベル(4)
1 返信

2,442件の閲覧回数
smbov
Contributor I

Finally, I could found the problem. I have to set the End Of Transfer Bit before each byte transfer.