Problem with LPC 2138 using J-Link

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem with LPC 2138 using J-Link

3,533 Views
gary_yang
Contributor II

We used J-link (JTAG interface) to connect to our circuit and could not connect successfully, as shown in figure 01.jpg

Our circuit design is shown in the figure 02.jpg,
Please help confirm. Is there any need for improvement? Or are there any other suggestions?

thank you

Regards,
Gary

Labels (1)
0 Kudos
Reply
1 Reply

3,431 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Gary Yang,

Thank you for your interest in NXP Semiconductor products and
the opportunity to serve you.
To provide the fastest possible support, I'd like to suggest you refer to the schematic of the ARM LPC2138 board.

Have a great day,
TIC

 

 

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

 

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply