Problem while debugging program. RFID module MF RC522.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem while debugging program. RFID module MF RC522.

1,657件の閲覧回数
robertchaim
Contributor I

Hello,

I use the LPC1769 and i have a problem that i can't deal with. It's my first time dealing with LPC programming.

After building a program i have no errors but when i run debugger there is :

"No source available for "semihost_exit() at 0x1f60".

The program is about reading RFID tag ID using module MF RC522. Program is downloaded from mbed.org and i'm using their libraries. Program was originally written for Arduino but after making few adaptations i managed (or not  ) to use it with my board. 

If you understood what i was trying to ask you about  please give me some advice because i have completely no idea how to do with it.

.175461_175461.jpgscreen błędu.jpg

Here is a screen of problems that pops up after running debugger.

Original Attachment has been moved to: RC522.zip

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,436件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Robert,

How did you imported the project to LPCXpresso? Maybe you could try creating a new cpp project in LPCXpresso and copy the source files to it.


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信