Problem to read a with lpcopen (LPC1837)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem to read a with lpcopen (LPC1837)

833件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by goffi on Mon Jul 21 08:03:11 MST 2014
I'm trying to read the sandisk sdcard i found in the evaluation board.

Using the latest lpcopen, when i read a sector (no matter which) ,my buffer is filled with only zeros (cid, csd are ok and no errors during the commands). Using the same program, i can read an unbranded sdcard and it works very nice.

The sample (dual device) works also with the sandisk card, but the libraries are different and is impossible to do some comparing.

Who can help me?
Thanks
ラベル(1)
0 件の賞賛
返信
0 返答(返信)