Problem in operating "UART" example with board OM13093

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem in operating "UART" example with board OM13093

1,430件の閲覧回数
rasheedkhankan
Contributor II

Hello friends,

I am using board OM13093 (contains LPC11c24).

When I am debugging the built-in example "nxp_lpcxpresso_11c24_periph_uart" with the "MCUXpresso IDE v10.0.2_411" and without any SDK; I can't see the initial messages on the console ???!!!

i.e. How can I mange the UART instructions without installed SDK???

 

Thanks in advance.

タグ(1)
0 件の賞賛
返信
1 返信

1,325件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Please check the below link and let me know if  this helps,

Printf debug and Semihosting on LPC 


Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信