Problem in operating UART example

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problem in operating UART example

1,749 次查看
rasheedkhankan
Contributor II

Hello friends,

I am using board OM13093 (contains LPC11c24).

When I am debugging the built-in example "nxp_lpcxpresso_11c24_periph_uart" with the "MCUXpresso IDE v10.0.2_411" and without any SDK; I can't see the initial messages on the console ???!!!

i.e. How can I mange the UART instructions without installed SDK???

Thanks in advance.

2 回复数

1,636 次查看
rasheedkhankan
Contributor II

Thanks a lot.

0 项奖励
回复

1,636 次查看
soledad
NXP Employee
NXP Employee

Hi,

Please check the below link and let me know if  this helps,

Printf debug and Semihosting on LPC 


Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------