Problem in operating UART example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem in operating UART example

1,729 Views
rasheedkhankan
Contributor II

Hello friends,

I am using board OM13093 (contains LPC11c24).

When I am debugging the built-in example "nxp_lpcxpresso_11c24_periph_uart" with the "MCUXpresso IDE v10.0.2_411" and without any SDK; I can't see the initial messages on the console ???!!!

i.e. How can I mange the UART instructions without installed SDK???

Thanks in advance.

2 Replies

1,616 Views
rasheedkhankan
Contributor II

Thanks a lot.

0 Kudos
Reply

1,616 Views
soledad
NXP Employee
NXP Employee

Hi,

Please check the below link and let me know if  this helps,

Printf debug and Semihosting on LPC 


Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------