Problem in implementation of SNMP Protocol with LPC1768

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problem in implementation of SNMP Protocol with LPC1768

3,723 次查看
pvgidveer
Contributor I

Hello everyone,

As mentioned in subject, I am working on a project in which SNMP protocol is to be implemented. I have written a code for SNMP Protocol which is working fine with the LPC1768 controller board. I am able to receive all the data(string) which is sent from controller to PC using ethernet. These strings are written in MIB_STR() function of MIB Table,

 

for eg.

const MIB_ENTRY snmp_mib[] = {

/* ---------- System MIB ----------- */

/* SysDescr Entry */
{ MIB_OCTET_STR | MIB_ATR_RO,
8, {OID0(1,3), 6, 1, 2, 1, 1, 1, 0}, 
MIB_STR("Hello World"),  //as this string i am not updating while execution of main function so it is working fine
NULL }

};

but when i am trying to update current values of parameters in place of string, it is not allowing to do that.

 

for eg.

const MIB_ENTRY snmp_mib[] = {

/* ---------- System MIB ----------- */

/* SysDescr Entry */
{ MIB_OCTET_STR | MIB_ATR_RO,
8, {OID0(1,3), 6, 1, 2, 1, 1, 1, 0}, 
MIB_STR(Temp[1]),  //error: initializer element is not a compile-time constant
NULL }

};

Temperature values are saved in an array in ASCII format. 

so, I am planning to Copy the same MIB Table to RAM when controller starts execution of code & then i want controller to read MIB table from the specific RAM address area so, i can update Current values of parameters at respective RAM Address locations.

may i know how to make controller to read from Specific RAM address location instead of  FLASH memory while execution of main function. 

Has anyone encountered this issue or maybe even found a solution?

Thank you.

Regards,

Pruthviraj Gidveer.

 

 

  

 

标签 (1)
0 项奖励
回复
4 回复数

3,714 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, PvgidVeer,

Can you tell us the tools you are using? is the MIB_STR(Temp[1])  a function or macro? do you have it's prototype?

BR

XiangJun Rong

0 项奖励
回复

3,707 次查看
pvgidveer
Contributor I

Hello, Xiangjun_rong,

I am using Keil uVision 4 IDE and MIB_STR() is declared as a macro in Net_Config.h file

macro declaration in Net_Config.h is as given below.


/* SNMP-MIB Macros */
#define MIB_STR(s) sizeof(s)-1, s 

 

Thanks & Regrads,

Pruthviraj Gidveer.

0 项奖励
回复

3,694 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Unfortunately, I do not see the Net_Config.h file in the LWIP directory, can you post all the project to the community so that we can have a review.

BR

XiangJun Rong

0 项奖励
回复

3,634 次查看
pvgidveer
Contributor I

Hi everyone,

Here i have attached a code, If you compile this code you will get an error, to resolve that error goto line no.49 of SNMP_MIB.c file & do modifications as mentioned in commented line then it will work. but actually i want to print the values of which are stored in dataString[]. If i try to print values from the array dataString[] it will give an error. Help me to resolve this problem.

 

Thanks & regards,

Pruthviraj Gidveer.  

0 项奖励
回复