Problem enabling interrupt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem enabling interrupt

983件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by djonesboni on Tue Jan 20 06:00:21 MST 2015
Hi

I am trying  to run FreeRTOS on LPC2366 but it seems timer0 is not interrupting (OS tick).

Setting a breakpoint in the tick handler, start debugging and the handler is never executed.

I tried enable interrupt on the processor (clear bits 6 and 7 of CPSR) but didn't work either.

I am using the default initialization and default handler of FreeRTOS tick.

Regards.
ラベル(1)
0 件の賞賛
返信
0 返答(返信)