Problem Programming LPC804 Xpresso Board using windows 11

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem Programming LPC804 Xpresso Board using windows 11

1,490 Views
Milix
Contributor I

Hi,

I am using McuXpresso on a windows 11 machine and I am trying to program the LPCXpresso804 board's MCU. The Probe is detected, but then an error indicates that the Probe is not open.

I have installed the windows USB driver for LPC probe LPC11Uxx_Debug_Probe_VCOM_v1.0.0.EXE, which indicates version 1.0.7 (Jully 2018) in its readme file.

The very same board with same cable can be easily programmed when using McuXpresso on a Ubuntu 20.04 machine, so the board is OK.

 

Does anyone is using a LPC Probe form windows 11 ? Is this a driver issue?

 

Thank you,

Milix

Tags (2)
0 Kudos
Reply
1 Reply

1,478 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

How about pressing ISP pin all the time when connecting?
If still have issue, please take a video or screenshot to show your steps.

 

BR

Alice

0 Kudos
Reply