Powerlib source code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Powerlib source code

Jump to solution
3,182 Views
alannilsson
Contributor II

Back in this thread, NXP announced it would publish the source code for the PowerLib required to setup the PLL correctly on the 546XX.  Has that happened?  Where is it at?

If NXP is unwilling/unable to provide said source code, will they provide the library in mach-o file format?

We are evaluating the 546XX for an upcoming project and the availability of either the source or a mach-o format is a deal breaker for us

Labels (1)
0 Kudos
Reply
1 Solution
2,953 Views
brendonslade
NXP TechSupport
NXP TechSupport

Update:

Due to customer interest / need for the library, we now include the source code for the power library in the SDK. For older products (like LPC546xx) we have an application note on the product page:

https://www.nxp.com/docs/en/application-note/TN00038.zip

Please carefully review the caveats to consider when making changes as these will affect power consumption and can impact product reliability if changed from recommended values used in the library.

 

Previous post below.

Hi Alan,

 

We don't normally publish this type of source because customers could make changes to internal device settings that could impact device characteristics, hence invalidating the datasheet information.

If you require more information due to your company's policies please contact us via your NXP sales contact (or distributor if you are not working directly with NXP) to make this request.

 

Regards,

Brendon

View solution in original post

0 Kudos
Reply
3 Replies
2,953 Views
soledad
NXP Employee
NXP Employee

Hi,

The LPC5410x power lib source has already been posted on web:

 https://www.nxp.com/docs/en/application-note/TN00026.zip

 

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,953 Views
alannilsson
Contributor II

That is for 541xx.  Is that the same as 546xx?

0 Kudos
Reply
2,953 Views
brendonslade
NXP TechSupport
NXP TechSupport

Update:

Due to customer interest / need for the library, we now include the source code for the power library in the SDK. For older products (like LPC546xx) we have an application note on the product page:

https://www.nxp.com/docs/en/application-note/TN00038.zip

Please carefully review the caveats to consider when making changes as these will affect power consumption and can impact product reliability if changed from recommended values used in the library.

 

Previous post below.

Hi Alan,

 

We don't normally publish this type of source because customers could make changes to internal device settings that could impact device characteristics, hence invalidating the datasheet information.

If you require more information due to your company's policies please contact us via your NXP sales contact (or distributor if you are not working directly with NXP) to make this request.

 

Regards,

Brendon

0 Kudos
Reply