Hello,
We are designing the implantable device using LPC55S1 MCU and want to bypass the internal DCDC converter to avoid using an inductor.
I have read this post on the forum and understood the requirement and the unused pin connection.
Still need to figure out what will be the proper power up sequence to supply the core voltage to MCU.
Both USB0 and USB1 are used and the VBAT = 1.8V in our design, hence we do have 3 distinct voltage rails: 1.8V(VBAT), 3.3V(USB), 1.1V(Core)
Could you please guide the proper powering up sequence in such case?
One additional question regarding using 1.2V for the core (I know it has already been discussed in the previous post) is that what would be the trade-off using 1.2V for all frequency range ( less than 100MHz), assuming that the supply is well controlled not to exceed the maximum rating of VDD_PMU (1.26Vmax_absolute)?

Best,
Jaehoon