Power down modes conflicting values

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Power down modes conflicting values

1,540 Views
vivienwong
Contributor I

Hi,

I am using the LPC1857 and I am referring to UM10430 Rev 2.8 dated 10 Dec 2015 and the deep power down modes in section 11.3.2 says that the values should be:

0x0030 00AA = Deep-sleep mode

0x0030 FCBA = Power-down mode

0x0033 FF7F = Deep power-down mode

In Section 11.4.1, the deep power-down mode is set to 0x0030FF7F which is conflicting with what is mentioned in Section 11.3.2

Also, when i downloaded the latest driver v2.1.8 (Release date: 5/27/2015) from

LPCOpen Software for LPC18XX|NXP

The pmc_18xx_43xx.h shows this:

* @brief Power Management Controller power modes

* Setting this mode will not make IO loose the state

*/

#define PMC_PWR_DEEP_SLEEP_MODE         0x3000AA

#define PMC_PWR_POWER_DOWN_MODE         0x30FCBA

#define PMC_PWR_DEEP_POWER_DOWN_MODE    0x30FF7F

/**

* @brief Power Management Controller power modes (IO powerdown)

* Setting this mode will make the IO loose the state

*/

#define PMC_PWR_DEEP_SLEEP_MODE_NO_IO         0x3F00AA

#define PMC_PWR_POWER_DOWN_MODE_NO_IO         0x3FFCBA

#define PMC_PWR_DEEP_POWER_DOWN_MODE_NO_IO    0x3FFF7F

Could you confim what should the deep-power-down mode value should be?

Also, what do you mean by the new settings  will not make IO loose state? Because based on section 11.2.5 of the user manual, deep power-down mode will lose the IO states. Does it mean that with this new setting (0x30FF7F or 0x33FF7F) the deep power down mode will NOT lose the IO states?

I need alot of clarification please :smileyhappy:

0 Kudos
Reply
1 Reply

1,369 Views
soledad
NXP Employee
NXP Employee

Hello Vivien,

Please check the below link: LPCOpen LPC43xx version release history and known issues | www.LPCware.com

You can find as known issues:

  • PMC_PWR_* definitions in the pmc_18xx_43xx.h file are not correct
    • PMC_PWR_DEEP_SLEEP_MODE is 0x3F00AA, should be 0x3000AA
    • PMC_PWR_POWER_DOWN_MODE is 0x3FFCBA, should be 0x30FCBA
    • PMC_PWR_DEEP_POWER_DOWN_MODE is 0x3FFF7F, should be 0x30FF7F


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply