Pn7462 Door Access with Stand By

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Pn7462 Door Access with Stand By

2,341 Views
gianlucapeterle
Contributor II

Hi, I am using phExDoorAccess application in stand by mode.

After the reset the microcontroller poll the evironment in LPCD mode correctly and if a card is detected it switch to full power mode.

My problem is that it happen once, after the card was detected for the first time and removed, the micro goes in stand by and stay there forever.

How can I put the micro in polling mode again?

Gianluca

Tags (1)
0 Kudos
Reply
1 Reply

2,015 Views
jimmychan
NXP TechSupport
NXP TechSupport

You can check the phExDoorAccess.c.

As the standby enabled (PHFL_ENABLE_STANDBY was defined), it will not go to the polling.

For example: in phExDoorAccess_SystemTask()

        case E_PH_CLIF:
            switch(sSysMsg.dwMsg[0])
            {
            /** CLIF application completed its task either go to standby OR start poll timer */
            case (uint32_t)E_PHEXDOORACCESS_CLIF_RSP_END:

#ifdef PHFL_ENABLE_STANDBY
                while(1)
                {
                    phLED_SetPattern(gkphLED_StandBy);
                    /** All the wakeup configurations are set by default in the EEPROM. */
                    phhalPcr_EnterLowPowerMode((phhalPcr_RfLdtParams_t *)gpkphCfg_EE_HW_RfLdtParams,
                        &phhalPcr_WakeUpConfig, &sStandbyPrevReason);
                    /** It is not expected to reach here, if so then wait for a while and try Standby. */
                    phRtos_TaskDelay(SYS_TASK_FREQUENCY_MS);
                }

#else
                phhalTimer_Start(gpphExDoorAccess_Clif_PollTimer, E_TIMER_SINGLE_SHOT);
#endif

So, you can try to modify the code to meet your needs.

0 Kudos
Reply