PinMux for LPC4078FBD100

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PinMux for LPC4078FBD100

2,379件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by akrylik on Thu Mar 27 22:36:36 MST 2014
Hi All

It seems that the PinMux tool for the LPC407x_8x series doesn't include the LQFP-100 package? Is there a more recent version somewhere or a way to add this chip on my own?

Kind regards,
Brian
ラベル(1)
0 件の賞賛
返信
6 返答(返信)

2,314件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by gjwep on Tue Feb 17 15:13:03 MST 2015
thanks a lot for the response - looking forward to the tool.

regards,
gj
0 件の賞賛
返信

2,314件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xianghuiwang on Tue Feb 17 14:20:11 MST 2015
hi, gjwep,

Sorry for the delay. We got response from the designer that it will be added in about two month time frame from now.
regards,
0 件の賞賛
返信

2,314件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by gjwep on Tue Feb 17 03:44:04 MST 2015
Just following up on this... I'd much appreciate any pointer to a pinmux or initializer (like e.g. http://www.lpcware.com/content/tools/lpc-initializer) that works for the LPC4078FBD100.

thanks&regards,
gj
0 件の賞賛
返信

2,314件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by akrylik on Sat Mar 29 03:01:57 MST 2014
Also would it be possible to release the pin/feature database so that we can write our own code-generation tools?
0 件の賞賛
返信

2,314件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by akrylik on Sat Mar 29 00:33:27 MST 2014
That's excellent news! Do you have a rough estimate of when it will be released?
0 件の賞賛
返信

2,314件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by embd02161991 on Fri Mar 28 11:15:48 MST 2014
Hi ,

This package is in the process of being added and the latest version will be released shortly.

Thanks,

NXP Technical Support
0 件の賞賛
返信