PinMux Bug in LPCOpen?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PinMux Bug in LPCOpen?

跳至解决方案
1,658 次查看
jamesm
Contributor II

I am using pin P1.25 on an LPC1759 as a Match Register output pin. The documentation shows only 3 functions for that pin, with MAT1[1] as the third. However, I set it as IOCON_FUNC2 (third function), I get no output. I get expected output on that pin if I set it to IOCON_FUNC3 with the function:

Chip_IOCON_PinMuxSet(pIOCON, 1, 25, IOCON_MODE_INACT | IOCON_FUNC3);

What am I missing?

Thanks in Advance - james

标签 (2)
标记 (1)
0 项奖励
回复
1 解答
1,546 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi James Massey,

According to the reference manual, the P1.25 work as the MAT1.1 when select the Function 3 instead of the Function 2, as the fig 1 illustrate.

2016-10-18_13-58-08.jpg

Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,547 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi James Massey,

According to the reference manual, the P1.25 work as the MAT1.1 when select the Function 3 instead of the Function 2, as the fig 1 illustrate.

2016-10-18_13-58-08.jpg

Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复