Pin compatibility between LPC4350 and LPC4370

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Pin compatibility between LPC4350 and LPC4370

994件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by JohnR on Wed Dec 04 06:28:36 MST 2013
Hi,

Looking through the manual, UM10503.pdf, I looks as if the LBGA26 versions of the LPC4350 and LPC4370 are identical with the exception of the new 12-bit ADC connections.

Could somebody (from NXP?) please let me know that this is right.

Thanks in advance,

JohnR



ラベル(1)
0 件の賞賛
返信
0 返答(返信)