Pin Interrupt on port 2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Pin Interrupt on port 2

1,552 Views
lak1
Contributor I

I just read in the documentation that Pin interrupt can be selected on alle GPIO pins on port 0 and port 1. Is there a way to implement this on Port 2 also (we are using Port 2 Pin 0)? 

In my project im using the Pin interrupt to mesaure the time in us, where the GPIO is low and don't know if there maybe is another way of solving this.

We are using a LPC1518JBD100.

Labels (3)
0 Kudos
Reply
1 Reply

1,509 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello Lasse Kristensen

 

Unfortunately, it is not possible to implement interruption on GPIO port 2, only port 0 and 1 are available for interruptions. I apologize for the inconvenience this may cause you.

 

If you have more questions do not hesitate to ask me.

Best regards,

Omar

0 Kudos
Reply