Pin Interrupt on port 2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Pin Interrupt on port 2

1,527件の閲覧回数
lak1
Contributor I

I just read in the documentation that Pin interrupt can be selected on alle GPIO pins on port 0 and port 1. Is there a way to implement this on Port 2 also (we are using Port 2 Pin 0)? 

In my project im using the Pin interrupt to mesaure the time in us, where the GPIO is low and don't know if there maybe is another way of solving this.

We are using a LPC1518JBD100.

ラベル(3)
0 件の賞賛
返信
1 返信

1,484件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello Lasse Kristensen

 

Unfortunately, it is not possible to implement interruption on GPIO port 2, only port 0 and 1 are available for interruptions. I apologize for the inconvenience this may cause you.

 

If you have more questions do not hesitate to ask me.

Best regards,

Omar

0 件の賞賛
返信