Phase locked loop

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Phase locked loop

2,366 Views
ianbenton
Senior Contributor I

Has anyone tried to make a phase locked loop out of one of the SCT timer? Has anyone succeeded?

I'd like to make SCT0 run in sync with the mains, because using the comparators as zero-cross detectors isn't that great on a noisy mains supply.

I tried computing the phase difference as SIN(2*PI*COUNT/MATCHREL)*COS(sampled input)-COS(2*PI*COUNT/MATCHREL)*SIN(sampled input) and then using the phase difference to adjust MATCHREL, but I can't get it to lock.

Any ideas? Is my sample rate (1600Hz) too low, or is the latency due to the period only updating after the next LIMIT event too long?

(The input is already a sinewave from the mains, and the cosine is found by taking a sample from quarter of a cycle ago.)

Labels (5)
0 Kudos
Reply
4 Replies

2,188 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Ian Benton ,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
Actually, I'm not very clear with your purpose, so I was wondering if you can introduce the scheme in details.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

2,188 Views
ianbenton
Senior Contributor I
0 Kudos
Reply

2,188 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Ian Benton,

Thanks for your reply.

I was wondering if you can share a compile-able demo which can replicate the phenomenon, it can help me to figure it out.

Looking forward to your reply.


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

2,188 Views
ianbenton
Senior Contributor I

My guess is that there could be two possibilities:
1) The mains sinewave has enough distortion that the result of the calculation never equals zero, even when the two signals are in phase.

2) There is too much latency due to MATCHREL only updating MATCH when the counter "limits".

I'll spend some more time experimenting, and possibly try a signal generator instead of the mains reference.

0 Kudos
Reply