(Penn State) Team ECHO Senior Design Project - Embedded Audio Mixer

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

(Penn State) Team ECHO Senior Design Project - Embedded Audio Mixer

3,180 次查看
meetparikh
Contributor I

Hello everyone in the LPC Forums; we’re seniors in Electrical Engineering from Penn State University. Our senior design class topic was Embedded Digital Audio, and our project is based on the LPCXpresso54608 that NXP graciously provided us. Thank you for that, and also for your prompt replies to our debug posts and messages about the board before it was available to the general public. Our project, Embedded Audio Mixer, is a graphical user interface derived from DJ mixing software, where we mix or cascade different Biquad filters such as Lowpass, Notch, and PeakingEQ, and allow the user to pick their own center frequency and Q factor to create a unique listening experience.

For our project, we used the Cirrus Logic Chip, the WM8904 onboard the device, and a custom graphics library running on the LCD Touchscreen.  The user selects when to start/stop the playback, pick a comfortable volume range, adjust filters type and their respective characteristics such as center frequency, dB Gain, etc., and add up to 3 filters in cascade. After the user selects the filters, we used interrupts to bring in audio data, process it and output it. This process is done in real time and therefore we limited the number of cascading filters to three.

Attached with this post is the Final Design Report detailing the project from concept to delivery. In addition, the links to our Youtube video demonstrating the project and the source code are listed below:

 

GitHub: https://github.com/MattPennock/Embedded-Audio-Mixer (Embeded Audio Mixer)

             https://github.com/MattPennock/Biquad (Biquad Filters Standalone)

             https://github.com/MattPennock/Interaction (Graphics Library Standalone)

 

Youtube: Team Echo- Embedded Audio Mixer Demo

3 回复数

2,938 次查看
jdibben
Contributor I

Thanks for posting this!

I loaded up the pre-built binary and this works fine but when I try building the project but it seems like the file containing main() is missing. The link process fails because there is an unresolved reference to main().

A source file called /source/Penumbra.c (and possibly other source files) seems to be missing from the repository on github?

0 项奖励
回复

2,938 次查看
brendonslade
NXP TechSupport
NXP TechSupport

Very nice guys - I'm going to try this one at home!

0 项奖励
回复

2,938 次查看
soledad
NXP Employee
NXP Employee

Hi,

Thank you for your input!!

Regards

Sol

0 项奖励
回复