PWM1 PCAP Inputs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PWM1 PCAP Inputs

1,980 次查看
rayaan
Contributor I

good day,

I am currently working on a project that is based on the lpc1764 mcu on custom board, I question is in connection with the PCAP functionality of the lp17 series, would it be possible to use the pcap functionality of pwm1, if I am already using pwm1.5 to generate a pwm signal. the reason for this is, that not all th I/O of the mcu has been routed out so I am quite restricted by the hardware.

Thanks in advance 

Rayaan

标签 (2)
0 项奖励
回复
2 回复数

1,841 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Rayaan Latief ,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.

would it be possible to use the pcap functionality of pwm1, if I am already using pwm1.5 to generate a pwm signal?

--Yes

Hope it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,841 次查看
rayaan
Contributor I

Thanks , I managed to get it working just made a silly mistake in the initialization of the pcap pin.

0 项奖励
回复