PWM channels for LPC43xx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PWM channels for LPC43xx

1,822 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tcmelco on Mon Sep 17 05:38:16 MST 2012
I am evaluating LPC43xx for my application. I need at least 6 PWM channels on it. NXP parametric search (http://www.nxp.com/parametrics/71562/) states that there is only one PWM channel (for motor control). But SCT also generates PWM, right? (as described on http://ics.nxp.com/support/microcontrollers/sct/).
So, I would like to know how many PWM channels I can configure on SCT. All the 16 outputs?
By the way, it is configurable, right? So I don't have to program interruptions on the microcontroller to check/change pin state.

Thanks in advance for any support.
Labels (1)
0 Kudos
Reply
4 Replies

1,726 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Paul on Tue May 21 07:32:54 MST 2013

We suggest that you use the Red State tool within LPCXpresso.
If you prefer not to use LPCXpresso, then you can use the Fizzim tool.  This tool can be found at <a href="http://www.lpcware.com/content/nxpfile/sct-tools">http://www.lpcware.com/content/nxpfile/sct-tools</a>.


-paul

0 Kudos
Reply

1,727 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by hlsa on Tue May 21 03:08:26 MST 2013

I tried to find the SCT-Tools on Lpcware.com, but I could not find them. Can anybody help me getting them?

0 Kudos
Reply

1,727 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tcmelco on Thu Sep 20 12:34:42 MST 2012
Thank you very much, Bavarian. That really answered my question.

Best regards,
tcmelco
0 Kudos
Reply

1,727 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bavarian on Tue Sep 18 02:57:22 MST 2012
Yes, the SCT can do PWM. There is an example attached. The SCT-Tools are available on lpcware.com, containing also other examples (which maybe do not perfectly fit to the latest hardware with regards to pin assignments).

In principle you could do PWM on all available outputs. Please check the documentation from the example.

Once configured the SCT runs without any processor interaction. So there is NO jitter.

Best regards,
NXP Support
0 Kudos
Reply