PWM SIGNAL GENERATION ON LPC54628

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PWM SIGNAL GENERATION ON LPC54628

ソリューションへジャンプ
1,627件の閲覧回数
aajithkumarr
Contributor I

Hi NXP TEAM,

I am currently working on a OM13098LPCxpresso54628 board. I am working on a PWM generation.

I have just created the example sdk file sctimer_simple_pwm in mcuxpresso ide. I have got the pwm output of 50% duty cycle and 24KHz pwm_freq. 

What is the maximum and minimum range of the pwm output. In user guide they have mentioned that the pwm output maximum will be 100MHz and not mentioned the minimum value. When I am practically implementing i can see the maximum output of 56MHz.and minimum of the 1Hz.

In user guide CLK_IN source is 12MHz and the PLL frequency = ((CLK_IN * M)/N)/2P.As mentioned in the user guide output frequency will be 4.3MHz to 550MHz.But the pwm maximum output will be 100MHz.

What is the mistake i have made with the calculation.What is the proper way to do this so and what is the maximum and minimum pwm output frequency.

Please guide me,

 

Thanks and regards,

A.Ajith Kumar.

0 件の賞賛
返信
1 解決策
1,617件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @aajithkumarr 

Do you mean "The maximum frequency for the SCTimer/PWM clock is 100 MHz." in UM as below?

Alice_Yang_0-1686041381886.pngAlice_Yang_0-1686041381886.png

 

There are two type of input for SCT, the the 100MHz clock limitation is only valid for the clock source inputted from external pads (SCT_IN7), if you use system clock as the SCTimer/PWM clock source, the system clock frequency can be greater than 100MHz.

Alice_Yang_1-1686041563711.pngAlice_Yang_1-1686041563711.png

 

 

The PWM output frequency can calculated after you choose source clock.

 

BR

Alice

元の投稿で解決策を見る

1 返信
1,618件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @aajithkumarr 

Do you mean "The maximum frequency for the SCTimer/PWM clock is 100 MHz." in UM as below?

Alice_Yang_0-1686041381886.pngAlice_Yang_0-1686041381886.png

 

There are two type of input for SCT, the the 100MHz clock limitation is only valid for the clock source inputted from external pads (SCT_IN7), if you use system clock as the SCTimer/PWM clock source, the system clock frequency can be greater than 100MHz.

Alice_Yang_1-1686041563711.pngAlice_Yang_1-1686041563711.png

 

 

The PWM output frequency can calculated after you choose source clock.

 

BR

Alice