PN5180 and LPC-Link2 programming

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN5180 and LPC-Link2 programming

1,785件の閲覧回数
Thomas_jjzhou
Contributor I

5a46fae66aedd418fa550f166cf4a28.jpgDear Sir,

As I starts to evaluate the PN5180 board, and connected with LPC-Link2. But not sucessfullly.

 

The console window shows:

41deb831be664a189c4af127e0cb2b5.pngeeff73ffcea04729cf30b70ea7fc79b.png

I ran the  NfcrdlibEx1_DiscoveryLoop code, but not show the card detected information .How to solve it? Thanks

タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,772件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Did you use MCU LINK test it? And has the similar issue?

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 件の賞賛
返信

1,763件の閲覧回数
Thomas_jjzhou
Contributor I

Yes, I connected the LPC-Link2 through cable.e3004795fd1be0621ecad2659e4f004.jpg

0 件の賞賛
返信