PIN configuration for ISP mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PIN configuration for ISP mode

1,611 Views
yangao
Contributor III

Hi,

In LPC55S1x/LPC551x datesheet, it says:

Function # 0

PIO1_2 — General-purpose digital input/output pin.
Remark: In ISP mode, this pin is set to the High Speed
SPI SCK function (Flexcomm 8).

Does it mean Function # need to be set to 0 to make this pin work as High Speed
SPI SCK function in ISP mode? If yes, how to set Function # for ISP mode? Can I set different Function # for ISP mode and non-ISP mode?

 

Regards,

Winston

Labels (1)
0 Kudos
Reply
1 Reply

369 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @yangao 

 

I have already replied to this question in another customer case. Please feel free to contact us if you have any further questions.

 

BR

Alice

0 Kudos
Reply