PIN INTERRUPT support package in LPCOpen for LPC1343

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PIN INTERRUPT support package in LPCOpen for LPC1343

1,362 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by safiullahh on Mon Jan 19 03:26:59 MST 2015
I see that within the file pinint_13xx.c there are no definitions for LPC1343.

The ifdef barrier is tagged to defined(CHIP_LPC1347) so I am assuming the definitions below are specific to the LPC1347 chip.

Is the chips LPC1343 not supported by LPCOpen 2.0? Or am I looking at the wrong file?

Regards.
Labels (1)
0 Kudos
Reply
1 Reply

1,321 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by embd02161991 on Wed Jan 28 23:41:24 MST 2015
Hi,

Please download the LPCOpen v2.05 for LPCXpresso LPC1343 board in the following link :
http://www.lpcware.com/content/nxpfile/lpcopen-software-development-platform-lpc13xx-packages

Thanks,
NXP Technical Support
0 Kudos
Reply