PID loop for LED driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PID loop for LED driver

1,567 Views
ranjithshanbhag
Contributor III

i am working on LED 40W driver with Fly-back followed by Digital Buck topology.

Operating output Current - 300mA to 1050mA

Operating output Voltage- 28V to 54V

i am finding 100Hz ripple contents at the LED output.

Buck current ADC conversation triggered with PWM. Every 7.69uS ADC will be sampled and 8 sample average will be calculated. Further moving average calculation of 13 samples will be done using 8 samples averaged value.

PID sampling time: 200uS

PID processing time: ~50-60uS

Can any one help me how to remove the 100Hz contents at LED output?

I attached High level circuit diagram, output current waveform and PID code.

pastedImage_1.png

pastedImage_2.jpg

// Count that gives the minimum target current of 20mA.
#define MINIMUM_ALLOWED_TARGET_

CURRENT_COUNT    (54 * 13)

uint32_t PI_output_current(uint32_t set, uint32_t actual)
{
    static int32_t previous_error = 0;

    static int32_t error_accumulated = 0;
    int32_t integral = 0;
    int32_t output = 0;
    int32_t derivative;
    static uint32_t previous_set = 0;

    // Cap the target current to minimum allowable current.
    if (set < MINIMUM_ALLOWED_TARGET_CURRENT_COUNT)
    {
        set = MINIMUM_ALLOWED_TARGET_CURRENT_COUNT;
    }

    if(set > 0)
    {

        if(previous_set != set)
        {
            previous_set = set;
            error_ignore = set * error_ignore_percentage;      // calculate 5% of the set point. Ignore if the error is less than that.
            error_ignore = error_ignore / 100;
        }
        error = set - actual;
        if(abs(error) > error_ignore) // only if the error is not acceptable do PID
        {
            error_accumulated += error;
            integral = (error_accumulated * (ADC_PI_Sample_time / 2)) / 10;

            derivative = error - previous_error;
            derivative = (derivative / (ADC_PI_Sample_time / 2)) / 10;

            if(integral > integral_limit)
            {

                integral = integral_limit;
            }

            if(integral < (int32_t)(0 - integral_limit))
            {
                integral = (int32_t)(0 - integral_limit);
            }

            output = (((int32_t)(KP * error) / (int32_t)10000) +
                      ((int32_t)(KI * integral) / (int32_t)10000) +
                      ((int32_t)(KD * derivative) / (int32_t)10000));

            if(abs(output) > MAX_DIFFERENCE_OF_OUTPUT)
            {
                if(output > 0)
                {
                    output = MAX_DIFFERENCE_OF_OUTPUT;
                }
                else
                {
                    output = (0 - MAX_DIFFERENCE_OF_OUTPUT);

                }
            }
            if((output < 0) && (output_to_set < abs(output)))
            {
                output_to_set = 0;
            }
            else
            {
                output_to_set += output;
            }
        }
        previous_error = error;

    }
    else
    {
        output_to_set = 0;
        previous_error = 0;
        integral = 0;
        error_accumulated = 0;
    }

    return output_to_set;
}

Tags (1)
0 Kudos
Reply
1 Reply

1,380 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Ranjith Shanbhag

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.

How's it going on now?

Have a great day,
TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply