PDRUNCFG

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PDRUNCFG

4,308件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by IanB on Fri Feb 19 05:57:40 MST 2016
What does bit 0 (IRC oscillator output) actually do, that makes it different from bit 1 (IRC oscillator)?

I mistakenly assumed that it was for the CLKOUT pin, and as I wasn't using the CLKOUT pin I switched it off, and it really didn't like being switched off!
ラベル(1)
0 件の賞賛
返信
9 返答(返信)

4,239件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by IanB on Wed Apr 20 00:43:34 MST 2016
Thanks. That makes a bit more sense of it, and explains why it all goes horribly wrong if I disable IRCOUT when I'm using the oscillator.
Probably, it's best if I don't start to wonder why anyone would want to enable or disable one without the other.
0 件の賞賛
返信

4,239件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by af_bln on Tue Apr 19 23:51:35 MST 2016
I would say
0 IRCOUT_PD IRC oscillator output power-down ===== disables the output amplifier after the oscillator stage
1 IRC_PD IRC oscillator power-down ===== disables the supply of the internal oscillator


0 件の賞賛
返信

4,239件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by IanB on Thu Apr 07 02:34:10 MST 2016
Unfortunately, I have just found that NXP restricts access to support to PC users and excludes those with Macs. The registration form doesn't work in Safari.
I thought I'd contact the webmaster to tell him, but first I have to register!
0 件の賞賛
返信

4,239件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Wed Apr 06 14:46:14 MST 2016
Try the NXP support?
https://nxpcommunity.force.com/community/communityLogin?pagename=communityContactSupport
0 件の賞賛
返信

4,239件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by IanB on Wed Apr 06 13:50:49 MST 2016
How do I get someone at NXP to pay attention and answer the question?
0 件の賞賛
返信

4,239件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by IanB on Sat Apr 02 01:13:27 MST 2016
So nobody knows what it does, then? Not even somebody at NXP?
0 件の賞賛
返信

4,239件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by IanB on Mon Mar 28 00:54:38 MST 2016

Quote:
It could help if you tell us what you are talking about (which register, which MCU).



1. The PDRUNCFG register (hence the title)

2. The LPC11xx MCU (hence this section of the forum) but the LPC8xx, LPC13xx and LPC15xx are the same.
0 件の賞賛
返信

4,239件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by starblue on Sun Mar 27 23:54:54 MST 2016
It could help if you tell us what you are talking about (which register, which MCU).
0 件の賞賛
返信

4,239件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by IanB on Sun Mar 27 14:34:17 MST 2016
So, does nobody know?
0 件の賞賛
返信