PCF8594 driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCF8594 driver

1,621 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Marqueses on Thu Aug 15 11:33:56 MST 2013
Hello,

I am trying to use the internal EEPROM from my lpcxpresso lpc1769 board. Has anyone a driver for this component using CMSIS?

Thanks in advance!
Labels (1)
0 Kudos
Reply
1 Reply

1,610 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Marqueses on Thu Aug 15 13:39:32 MST 2013
It is ok if the driver is from another device with i2c communication. I just want to see how to use i2c functions from CMSIS, which I can't understand at all. The most strange thing for me is the use of the same function to write and read the eeprom depending in the i2c struct configuration...

Thanks!
0 Kudos
Reply