Operation speed of MCU is different.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Operation speed of MCU is different.

1,041件の閲覧回数
HungNguyenDQ
Contributor I

I use Keil C V5 to upload code to MCU LPC2368. Firstly, I upload code to MCU LPC2368(1). Then I replace MCU LPC2368(1) on board by MCU LPC2368(2) . I upload code(the same as before) to MCU LPC2368(2). But MCU LPC2368(1) and MCU LPC2368(2) are different in running. Speed of running is defferent.

Note: MCU LPC2368(2) were uploaded other code before.

Please help me reply question below:

1. Code (be uploaded before) effect to speed of MCU?

2. When I upload new code, all setting of previous code will be erase?

3. Why are speed of running defferent?

Please help me!!

タグ(1)
0 件の賞賛
返信
1 返信

1,033件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

First of all, when you upload new application code to flash, the previous code are erased and updated with new code.

Regarding your code, it appears that the delay function is ambiguous, pls try to use the following code:

void msdelay(unsigned int time)
{
unsigned int i,j;
for(i=0; i<time; i++) {}
for(j=0;j <6002; j++) {}
}

or


void msdelay1(unsigned int time)
{
unsigned int i,j;
for(i=0; i<time; i++)
{
for(j=0;j <6002; j++)
{
__asm("nop");
}
}
}

do you know that MCU runs in different speed by observing the GPIO toggling in different frequency with the same code?

BR

XiangJun Rong

0 件の賞賛
返信