OpenLPC and SCTPWM on LPC11E67

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OpenLPC and SCTPWM on LPC11E67

1,803件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by WHLShort on Wed Dec 03 15:09:40 MST 2014
I have now been struggling with the SCT and PWM for some time.
What I would like is to be able to generate a simple PWM signal on Port 2.2 (SCT0_1) and Port 1.13 (SCT0_3) that are independen of each other.
In the example below I have configured the clock to be at 2MHz (core at 48M). Dividing that into 1000 makes the PWM tick occur at 2kHz.
Using the code below makes my system trig the interrupt, but the output pins are NOT trigged. I have added two notes with "// NECESSARY?", and they can set and clear the pin (PIO2_2) as desired, but the flanks are not always as intended - changes. Anyhow the main issue is, that the output pins are not set in the code eventhough the Chip_SCT_SetOutput  and Chip_SCT_ClearOutput-functions are used ?!?

Idea and inputs are appreciated! 

#include "chip.h"

/**
 * @briefHandle interrupt from State Configurable Timer
 * @returnNothing
 */
void SCT0_1_IRQHandler(void)
{
/* Clear the Interrupt */
volatile uint32_t flag = Chip_SCT_GetEventFlag(LPC_SCT0);

if(flag & SCT_EVT_0)
{
LPC_SCT0->EVFLAG = SCT_EVT_0;
//Chip_GPIO_SetPinState(LPC_GPIO, 2, 2, 1);// NECESSARY?
}
if(flag & SCT_EVT_1)
{
LPC_SCT0->EVFLAG = SCT_EVT_1;
//Chip_GPIO_SetPinState(LPC_GPIO, 2, 2, 0);// NECESSARY?
}
if(flag & SCT_EVT_3)
{
LPC_SCT0->EVFLAG = SCT_EVT_3;
}
}


void SCT0_Init(void)
{
// enable clock for SCT0
Chip_SCT_Init(LPC_SCT0);

Chip_IOCON_PinMuxSet(LPC_IOCON, 2, 2, 0x00000083);            // PIO2_2  as SCT0_OUT1
Chip_IOCON_PinMuxSet(LPC_IOCON, 1,13, 0x00000082);            // PIO1_13 as SCT0_OUT3
//    Chip_GPIO_SetPinDIROutput(LPC_GPIO, 2, 2);                                  // Set as output pin - should not be necessary
//    Chip_GPIO_SetPinDIROutput(LPC_GPIO, 1,13);                                  // Set as output pin - should not be necessary

Chip_SCT_Init(LPC_SCT0);   // Enable clock for SCT0/1

Chip_SCT_Config(LPC_SCT0, SCT_CONFIG_32BIT_COUNTER | SCT_CONFIG_AUTOLIMIT_L);// two 16-bit timers, clocked internally, auto limit

Chip_SCT_SetControl(LPC_SCT0, SCT_CTRL_PRE_L(24));                        // Prescaler = 24@Core=48M => SCT clock = 2 MHz

Chip_SCT_SetMatchCount (LPC_SCT0, SCT_MATCH_0, 1000);   // match 0 @ 10/2MHz = 5 usec (100 KHz PWM freq)
Chip_SCT_SetMatchReload(LPC_SCT0, SCT_MATCH_0, 1000);

Chip_SCT_SetMatchCount (LPC_SCT0, SCT_MATCH_1, 600);       // match 1 used for duty cycle
Chip_SCT_SetMatchReload(LPC_SCT0, SCT_MATCH_1, 600);

Chip_SCT_SetMatchCount (LPC_SCT0, SCT_MATCH_3, 300);       // match 3 used for duty cycle
Chip_SCT_SetMatchReload(LPC_SCT0, SCT_MATCH_3, 300);

Chip_SCT_EventState(LPC_SCT0, SCT_EVENT_0, ENABLE_STATE0);// event 0 only happens in state 0
Chip_SCT_EventControl(LPC_SCT0, SCT_EVENT_0, (CHIP_SCT_EVENTCTRL_T) ( SCT_EVECTRL_MATCH0    |// related to match 0
  SCT_COMBMODE_MATCH|// COMBMODE[13:12] = match condition only
  SCT_STATELD_1    |// STATELD[14] = STATEV is loaded into state
  SCT_STATEEV_0        ));// STATEV[15] = 0

Chip_SCT_EventState(LPC_SCT0, SCT_EVENT_1, ENABLE_STATE0);// event 1 only happens in state 0
Chip_SCT_EventControl(LPC_SCT0, SCT_EVENT_1, (CHIP_SCT_EVENTCTRL_T) ( SCT_EVECTRL_MATCH1    |// related to match 1
  SCT_COMBMODE_MATCH|// COMBMODE[13:12] = match condition only
  SCT_STATELD_1    |// STATELD[14] = STATEV is loaded into state
  SCT_STATEEV_0    )); // STATEV[15] = 0

Chip_SCT_EventState(LPC_SCT0, SCT_EVENT_3, ENABLE_STATE0);// event 3 only happens in state 0
Chip_SCT_EventControl(LPC_SCT0, SCT_EVENT_3, (CHIP_SCT_EVENTCTRL_T) ( SCT_EVECTRL_MATCH1    |   // related to match 1
  SCT_COMBMODE_MATCH|// COMBMODE[13:12] = match condition only
  SCT_STATELD_1    |// STATELD[14] = STATEV is loaded into state
  SCT_STATEEV_0    ));// STATEV[15] = 0

Chip_SCT_SetOutput(LPC_SCT1, SCT_OUTPUT_1, SCT_EVT_0);// event 0 will set SCTx_OUT0
Chip_SCT_ClearOutput(LPC_SCT1, SCT_OUTPUT_1, SCT_EVT_1);// event 1 will clear SCTx_OUT0

Chip_SCT_SetOutput  (LPC_SCT0, SCT_OUTPUT_3, SCT_EVT_0);// event 0 will clear SCT_OUT3
Chip_SCT_ClearOutput(LPC_SCT0, SCT_OUTPUT_3, SCT_EVT_3);// event 3 will set SCT_OUT3

/* Enable an Interrupt on the Match Event */
Chip_SCT_EnableEventInt(LPC_SCT0, SCT_EVT_0);
Chip_SCT_EnableEventInt(LPC_SCT0, SCT_EVT_1);
Chip_SCT_EnableEventInt(LPC_SCT0, SCT_EVT_3);

/* Enable the IRQ for the SCT */
NVIC_EnableIRQ(SCT0_1_IRQn);

// unhalt it by clearing bit 2 of the CTRL register
Chip_SCT_ClearControl(LPC_SCT0, SCT_CTRL_HALT_L);
}
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,663件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by WHLShort on Sun Dec 07 05:24:34 MST 2014
Thank you for the advise....

An idea for the projects in the future might be to add a _single_ image of the states.
0 件の賞賛
返信

1,663件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Fri Dec 05 19:51:02 MST 2014
Hi WHLShort,
I did not go through your code but I suggest you to read and use example from SCTimer/PWM cookbook. You can download this cookbook from
http://www.lpcware.com/category/project-categories/sct

It contains example for LPC11xx,
0 件の賞賛
返信