OM13092 "Cannot halt processor" on the target LPC54608

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OM13092 "Cannot halt processor" on the target LPC54608

ソリューションへジャンプ
3,914件の閲覧回数
k2
Contributor III

Help - I'm using the OM13092 Development board to integrate my LPC54608 board design.

I re-arranged the clock order for USB and then got this.

I put the working code back the way it should be ... but now i'm stuck without a target debugger.

I can program and run the onboard LPC54608 but it won't fully connect to the off board target LPC54608.

I've seen this problem across other NXP development boards. 

Is there a standard way to restore the link2 functionality back to the way it was ?

I looked thru the documentation and it doesn't say how to recover from this problem.

It has been working great for the last 3 months. Pretty sure it was the USB clock tweak i was trying that did this.

This is really setting me back ... I hope there is some documentation showing how to restore the Link2.

I tried the script - program_CMSIS - didn't help unlock it.

Is there a magic script somewhere to unlock this ? 

Kevin

0 件の賞賛
返信
1 解決策
1,517件の閲覧回数
k2
Contributor III

Resolved by replacing the LPC54608 chip.

Bricked it somehow (misplaced the clock statement) , and don't have a way to unbrick it with ISP settings without a hardware mod.

After replacing the chip - back to normal.

ugly and unforgiving mistake on my part.

Kevin

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,518件の閲覧回数
k2
Contributor III

Resolved by replacing the LPC54608 chip.

Bricked it somehow (misplaced the clock statement) , and don't have a way to unbrick it with ISP settings without a hardware mod.

After replacing the chip - back to normal.

ugly and unforgiving mistake on my part.

Kevin

0 件の賞賛
返信