OM13092/J14 expansion header's SPI interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OM13092/J14 expansion header's SPI interface

896件の閲覧回数
belmontbob59
Contributor IV

I am confused about the documentation. It reads:

pastedImage_1.png

This does not mention JS34 or JS35 for FC3's MISO/MOSI However the schematic has this for J14:

pastedImage_4.png

and this for the MCU:

pastedImage_2.png

And this:

pastedImage_3.png

So by default the MCU FC3's MISO/MOSI pins are routed to the SDRAM correct? This means that I can not use J14 extension header FC3. But the documentation (table 14 just above) does not mention to modify JS34 and JS35. Further more the table "JS33, JS34,JS35,JS36"  reads to shunt JS34/JS35 in position 2-3 (default) when using 3.3V.

So does this means that the expansion port J14 can not be used? 

Please advise

ラベル(1)
0 件の賞賛
返信
0 返答(返信)