OM13086

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OM13086

2,228件の閲覧回数
zhouhaohua
Contributor I

I just bought NXP OM13086 Kits, but I cannnot see the tutorials to make the default cloud connection function, please guide how to do that?  first time user, I cannot find any document to follow, some time point to Zentri,  but I don't know the full step.

    right now I can see temperature on the screen, but I don't know how to connect it to cloud and how to show the temperature in the web browser.

0 件の賞賛
返信
2 返答(返信)

2,080件の閲覧回数
zhouhaohua
Contributor I

LPCXpresso v8.2.2 [Build 650] [2016-09-09]  Log file shows failed on OM13086SCCK

01:47:46.178 [INFO] Is the device connected and correctly enumerated?
01:47:46.194 [INFO] Checking for solution ...
01:47:46.194 [INFO] Retrieving driver nodes ...
01:47:46.663 [INFO] NXP driver repair available
01:47:50.782 [INFO] Attempting to repair NXP driver issue
01:47:57.421 [INFO] Retrieving driver information ...
01:47:57.421 [INFO] Retrieving driver nodes ...
01:47:57.801 [INFO] Success
01:47:57.801 [INFO] Generating repair script1
01:47:57.801 [INFO] Executing repair script part1, must run as Admin, click 'Yes' to prompt
01:48:37.493 [INFO] Success
01:48:37.496 [INFO] Verifying repair step
01:48:37.496 [INFO] Retrieving driver nodes ...
01:48:42.884 [INFO] Executing repair script part2, must run as Admin, click 'Yes' to prompt
01:48:44.740 [INFO] Success
01:48:58.928 [INFO] Retrieving driver nodes ...
01:49:04.7 [INFO] Generating repair script
01:49:04.7 [INFO] Executing repair script part3, must run as Admin, click 'Yes' to prompt
01:49:05.683 [INFO] Success
01:49:14.295 [INFO] Retrieving driver nodes ...
01:49:19.706 [ERROR] Error while verifying driver
01:49:19.706 [ERROR] Exception: Platform code: OM13086SCCK not supported
01:49:21.19 [INFO] Optionally, try re-installing the LPCXpresso drivers:
1. Open the folder: c:\nxp\LPCXpresso_XXX\Drivers
2. Double-click lpc_driver_installer.exe
3. Choose the "Remove" option from the dialog
4. Double-click lpc_driver_installer.exe again
5. Choose the "Install" option
01:49:59.815 [INFO] Error while verifying driver

0 件の賞賛
返信

2,079件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Charlie,

This problem seems to be related with the Zentri plugin, I would recommend you to contact Zentri directly:

Support – Zentri 

Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信