OM13086 Firmware and default setting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OM13086 Firmware and default setting

17,175 Views
zhouhaohua
Contributor I

I have bought a NXP-zentri cloud kits OM13086, but I think my  default firmware might be damaged, please help on these issues

  1. where to get the default firmware

  2 how to program the firmware into the EVB board

 3. what is the default Jumper location

0 Kudos
Reply
3 Replies

17,017 Views
randylathropade
Contributor I

I also have this issue, of not being able to successfully pass the "Setup Device & SDK" step

0 Kudos
Reply

17,017 Views
soledad
NXP Employee
NXP Employee

Hi charlie zhou,

You can download a software development kit from the ZENTRI developer portal for NXP:

NXP – Zentri 

The Default jumper positions are shown in red: 

pastedImage_3.png

You can find more information about the jumper settings and debug configurations in the following user manuals:

https://www.lpcware.com/system/files/UM10946-om13084_88.pdf 

https://www.lpcware.com/system/files/UM10940-om13082_1.0_0.pdf 

I hope this helps,


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

17,016 Views
zhouhaohua
Contributor I

Dear SOL:

I have install the ZentriSDK correctly, but I cannot pass the

"ZentriOS"->setup device and SDK step,

the " NXP driver repair utility" keep showing up and failed on "verify

driver" step

I do find the "repair-script1" certificate expire 11/18/2016, but I

am not sure if it is because the certificate expire or not.

another quesiton related with the script need "administrator

privilege", I am admin, but I don't know if runs in admin right or not

this is orginal kits I bought from digikey, I expected it can directly

work and NXP have step by step document,but I cannot find it.

this kits is really hard to use, I am using windows 10 and LPC IDC 8.2.2

0 Kudos
Reply