OM13069 source code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OM13069 source code

1,541件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by j800514 on Thu Mar 17 04:51:24 CDT 2016
I have download "NXP_Quick_Jack_LPC800_Keil_IAR.zip" and "NXP_Quick_Jack_LPC800_LPCXpresso.zip"


in the keil , i can't rebuild the code.
build out:
".\keil_output\nxp_quick_jack_app.axf: error: L6002U: Could not open file ...\..\..\..\..\software\lpc_core\lpc_chip\chip_8xx\keil_output\chip_8xx_lib\chip_8xx_lib.lib: No such file or directory
Finished: 0 information, 0 warning, 0 error and 1 fatal error messages.
".\keil_output\nxp_quick_jack_app.axf" - 1 Error(s), 0 Warning(s)."


in the LPCXpresso V7.1.1_125 debug
it pop up error
Error in final launch sequence
Error: Error reported by server (redlinkserv.exe):
RedlinkAPI: Hardware interface transfer error
CMSIS-DAP will be restarted.
Please restart your debug session.
Error: Error reported by server (redlinkserv.exe):
RedlinkAPI: Hardware interface transfer error
CMSIS-DAP will be restarted.
Please restart your debug session.


in the LPCXpresso current version debug(use redlink)
it pop up error
02: Failed on connect
02: Failed on connect
Invalid probe index.
31: No connection to emulator device

PS. i use lpc link2
I have try my code can debug
is source code problem?
or what can i do?
ラベル(1)
0 件の賞賛
返信
1 返信

1,449件の閲覧回数
lpcware
NXP Employee
NXP Employee
bump
0 件の賞賛
返信