OM13021 debugging

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OM13021 debugging

1,854 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jujosaar on Thu Mar 10 01:53:47 MST 2016
Hi!

I bought the OM13021: NGX LPC11U14 Evaluation Board

It should feature an on-board debugger and should be SWD debuggable through CooCox_CoIDE.

Problem is, CoIDE doesn't support the LPC11U14 nor does the LPCExpresso support the on-board debugger.
The on-board debugger isn't recognized by Windows 7 64bit and the external drivers didn't help either (ColinkExUsbDriver, the device is identified by windows as "other device" under the name COOCOX COLINKEX).

I also tried Keil uVision ver. 4 and ver. 5. That didn't work either since the debugger isn't listed and I don't know which one to use.

On top of everything, the drivers, the IDE and everything else is either deprecated or very old.

This board is advertised as an LPCXpresso board by some distributors and I find it highly misleading.


Seriously speaking: I've spent a good two working days trying to get a simple blink to compile and debug on the board without success.
I'd really, really, really like a refund or a WORKING evaluation board of the LPC11U14 MCU.
Labels (1)
0 Kudos
Reply
2 Replies

1,746 Views
tombuil
Contributor II

Hello Guys,

I have the same LPCexpresso OM13021 from mouser. And the same problems as jujosaar!

I was already wondering why the USB connector on the LPC11U14 side, so I mounted my own.

After trying to upload the software from LPCexpresso I got a bad surprise... nothing!

Downloading the drivers from http://www.coocox.com/  results in 404 errors.

Edit:

After reading this things become clear, took a while before I found it tho:

https://www.coocox.org/wiki/coocox/CoLinkEx/CoLinkEx-User-Guide

0 Kudos
Reply

1,746 Views
lpcware
NXP Employee
NXP Employee
bump
0 Kudos
Reply