OM11043 (LPC1768 Dev Board) Debug Connector?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OM11043 (LPC1768 Dev Board) Debug Connector?

2,245件の閲覧回数
johnwhitmore
Contributor III

I'm looking at the NXP OM11043 LPC1768 Dev Board [1] but can't see a JTAG, or SWD  Connector. I want to try things out both programming an LPC device and also using the various debugging tools.

Is this a case of going through the Datasheet for the LPC1768 and working out which pins on the 40 pin 0.1" header are required for a debug header and connecting them to a connector suitable for a J-Link style device. I'm sure I must be missing something as surely a Dev board would have a JTAG Interface?

[1] http://www.farnell.com/datasheets/866692.pdf 

タグ(1)
2 返答(返信)

2,027件の閲覧回数
johnwhitmore
Contributor III

Thanks a million Carlos, ordered that up. Thanks again for your help

2,027件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi John,

This ARM MBED board does not have a SWD or JTAG connector, it has a built-in USB programming interface that is as simple as using a USB Flash Drive. You can find the schematics and additional information about the board on this link:

https://developer.mbed.org/platforms/mbed-LPC1768/

If you want a development board with a SWD connector for external debug probes then I would recommend you to use our LPCXpresso board for LPC1769 with CMSIS DAP probe:

http://www.nxp.com/products/microcontrollers-and-processors/arm-based-portfolio/lpc-cortex-m-mcus/so...


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer