OM 13069 - adding sensors

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OM 13069 - adding sensors

1,052 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by parithosh93 on Mon Mar 21 23:06:47 MST 2016
I have built the source code given and identified if it is working on the mobile phone as well. But now i would like to add my own sensors to that. In order to read soil moisture and humidity.
From what i read, i am supposed to connect the sensors to the expansion I/O pins and then edit the source code.

But my question is if i should edit the firmware in any way to make it read data from the extra pins as well? And then accordingly edit the source code?

It would be great if someone could point me in the right direction.
Labels (1)
0 Kudos
Reply
1 Reply

1,037 Views
lpcware
NXP Employee
NXP Employee
bump
0 Kudos
Reply