[Not the usual] PLL initialisation question (LPC1768)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[Not the usual] PLL initialisation question (LPC1768)

1,634 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by DiBosco on Fri Apr 26 04:25:38 MST 2013

I have inherited some code from someone for the LPC1768. In the PLL initialisation he has some really ugly code that jumps to a reset vector if the PLL's registers aren't set to the correct values and just tries again until it works. I'm just not having that as a valid way of working (quite aside from having gotos in C), it just can't be the right way of initialising the peripheral.

However, if I do not follow this reset procedure, I simply cannot get the PLLSTAT register to hold anything other than 0 and I'm stuck waiting for the PLL initialise, which it never does. The IAR examples show you how to set up all peripherals other than, as far as I can see, the PLL, so I can't go and look there for help.

I printed out 4.5.13 of the user manual and followed the nine steps, but never get past the PLL being initialised. Anyone able to help please? I have the code below.

If anyone has a snippet of the relevant part of the code that works for them it would be useful too. As far as I can see I have no forgotten to initialise something else necessary, but maybe that's all it is?

Thanks a lot.

------------------------------------------------------------------------------------


// Step 1 - Disconnect PLL        
    LPC_SC->PLL0CON &= ~CLKPWR_PLL0CON_CONNECT;   // Disconnect PLL0
    LPC_SC->PLL0FEED |= 0xAA;
    LPC_SC->PLL0FEED |= 0x55;
// Step 2 - Disable PLL
    LPC_SC->PLL0CON &= ~CLKPWR_PLL0CON_ENABLE;   // Disable PLL0
    LPC_SC->PLL0FEED |= 0xAA;
    LPC_SC->PLL0FEED |= 0x55;
// step 3 - Change clock divisor
    LPC_SC->CCLKCFG = 0x02;  //Set the divider (to 3-see calcs below)
// Step 4 - Change the clock source       
    LPC_SC->SCS &= 0x00000060; //Set up the external clock. We have a 12MHz Xtal - Set B4 low   
    LPC_SC->SCS |= 0x00000020;    //Start EXTOSC   
    while(!LPC_SC->SCS & 0x00000040);  //And wait for it to become stable
//Select XTAL as the clock source input to PLL
    LPC_SC->CLKSRCSEL = CLKPWR_CLKSRCSEL_CLKSRC_MAINOSC;
// Step 5 - Write to PLL0CFG, this sets multiply and divide values.
// 12MHz crystal giving 96MHz clock
// Target PLL output would therefore be 288MHz
// Maths is ((Ctarg)288*1000000*1)/(2*(XTAL)12*1000000)=12=0x0C
// This gives us a divider of 1 and a multiplier of (N-1,M-1)0x0B
    LPC_SC->PLL0CFG = 0x0B;
    LPC_SC->PLL0FEED |= 0xAA;
    LPC_SC->PLL0FEED |= 0x55;   
// Step 6 - Enable PLL
    LPC_SC->PLL0CON = CLKPWR_PLL0CON_ENABLE;  
    LPC_SC->PLL0FEED |= 0xAA;
    LPC_SC->PLL0FEED |= 0x55;       
// Step 7 - already done in step 3
   
// Step 8 - Wait for PLL to lock   
    while ((LPC_SC->PLL0STAT & CLKPWR_PLL0STAT_PLOCK) == 0);        <---always stuck here
// Step 10 - Connect the system clock to the PLL
    LPC_SC->PLL0CON |= CLKPWR_PLL0CON_CONNECT;   // Connect PLL0 now it is locked
    LPC_SC->PLL0FEED |= 0xAA;
    LPC_SC->PLL0FEED |= 0x55;

Labels (1)
0 Kudos
Reply
1 Reply

1,585 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Paul on Mon May 06 11:47:00 MST 2013

I would recommend that you look at the LPC17xx example code we have available for download from:
<a href="http://www.lpcware.com/node/11538/129">http://www.lpcware.com/node/11538/129</a>
Take a look at the system_LPC17xx.c file for details.
The only thing I could see as a potential problem were the statements:
LPC_SC-&gt;PLL0FEED |= 0xAA;
LPC_SC-&gt;PLL0FEED |= 0x55;
Note that the PLL0FEED register is a write-only register, so the feed sequence should be:
LPC_SC-&gt;PLL0FEED = 0xAA;
LPC_SC-&gt;PLL0FEED = 0x55;

0 Kudos
Reply