Not able to select BSP for LPC54628 in Appwizard

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Not able to select BSP for LPC54628 in Appwizard

1,828 Views
Sajil
Contributor I

I am attempting to build a GUI application on LPC54628 board. While creating the project, BSP selection is required in which I have no option coming up for the board. The GUI can be built but the code cannot be generated for integration with MCUexpresso. 

I am following the links mentioned below:

@https://www.nxp.com/design/training/mcu-tech-minutes-gui-development-with-emwin-and-appwizard:TIP-M...

@https://www.nxp.com/design/software/embedded-software/nxp-emwin-libraries:EMWIN-GRAPHICS-LIBRARY

I have made sure the emwin is ticked in the SDK builder for MCUexpesso and have repeated the process multiple times but in vain.I  have attached the screenshot for reference.BSP selection is emptyBSP selection is empty

Please help me with this issue, Thanks.

Labels (2)
0 Kudos
Reply
1 Reply

1,808 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Sajil,

 

I was able to confirm the same result, and report it to SE team, they help to confirm whether it will be updated on our end with the latest version. 

Now on Segger's website for their trial versions, The 1.22 and 1.24 have the BSP information intergrated again. I recommend that if you needs it right away they can begin to develop your application using the trial version from Segger's website. Or create custom BSP refer to AppWizard-> 12.2 Creating custom BSPs .

 

BR

Alice

 

0 Kudos
Reply