Not able to select BSP for LPC54628 in Appwizard

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Not able to select BSP for LPC54628 in Appwizard

1,810件の閲覧回数
Sajil
Contributor I

I am attempting to build a GUI application on LPC54628 board. While creating the project, BSP selection is required in which I have no option coming up for the board. The GUI can be built but the code cannot be generated for integration with MCUexpresso. 

I am following the links mentioned below:

@https://www.nxp.com/design/training/mcu-tech-minutes-gui-development-with-emwin-and-appwizard:TIP-M...

@https://www.nxp.com/design/software/embedded-software/nxp-emwin-libraries:EMWIN-GRAPHICS-LIBRARY

I have made sure the emwin is ticked in the SDK builder for MCUexpesso and have repeated the process multiple times but in vain.I  have attached the screenshot for reference.BSP selection is emptyBSP selection is empty

Please help me with this issue, Thanks.

ラベル(2)
0 件の賞賛
返信
1 返信

1,790件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Sajil,

 

I was able to confirm the same result, and report it to SE team, they help to confirm whether it will be updated on our end with the latest version. 

Now on Segger's website for their trial versions, The 1.22 and 1.24 have the BSP information intergrated again. I recommend that if you needs it right away they can begin to develop your application using the trial version from Segger's website. Or create custom BSP refer to AppWizard-> 12.2 Creating custom BSPs .

 

BR

Alice

 

0 件の賞賛
返信