Not Getting Proper Status Responses of Repeated Start in I2C Protocol of LPC1343?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Not Getting Proper Status Responses of Repeated Start in I2C Protocol of LPC1343?

835件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xpress_embedo on Wed Jul 09 10:05:49 MST 2014
Hello!! Everyone i am working on LPC1343 Micro-controller and wants to interface RTCC PCF8523 with LPC1343.

I write code for I2C protocol but its not working.
The problem is found when i send repeated start from master (LPC1343), the status for this must be 0x10 while i am getting 0x28 every time.

[COLOR="#008000"][SIZE=4]I am attaching my code in the zip file available below.[/SIZE][/COLOR]

The functions used for I2C Protocol are as follow:-

[syntax=c]

#include "LPC13xx.h"
#include "I2C.h"
#include "UART.h"

void I2C_Init(unsigned char Mode)
{
LPC_SYSCON->PRESETCTRL |= (1<<1);//De-Asserts Reset Signal to I2C
LPC_SYSCON->SYSAHBCLKCTRL |= (1<<5);//Enable I2C Clock

LPC_IOCON->PIO0_4 &= ~0x3F;
LPC_IOCON->PIO0_4 |= 0x01;//SCL

LPC_IOCON->PIO0_5 &= ~0x3F;
LPC_IOCON->PIO0_5 |= 0x01;//SDA

if(Mode == I2C_SPEED_400)
{
LPC_I2C->SCLH = 90;//I2PCLK is 72MHz
LPC_I2C->SCLL = 90;//I2PCLK is 72MHz
}
else if(Mode == I2C_SPEED_100)
{
LPC_I2C->SCLH = 360;//I2PCLK is 72MHz
LPC_I2C->SCLL = 360;//I2PCLK is 72MHz
}

LPC_I2C->CONCLR = 0xFF;//Clear All Flags
LPC_I2C->CONSET = (1<<6);//I2C Interface Enable
}
void I2C_Start(void)
{
LPC_I2C->CONSET |= 0x20;//Set the Start Bit
while(LPC_I2C->STAT!=0x08);//Wait for the Status Bit
}
void I2C_Restart(void)
{
LPC_I2C->CONSET |= 0x20;//Set the Start Bit
while(LPC_I2C->STAT!=0x10);//Wait for the Status Bit
}
void I2C_Stop(void)
{
LPC_I2C->CONSET |= 0x14;//Stop I2C
LPC_I2C->CONCLR = 0x08;
}
void I2C_Write(unsigned char data,unsigned char status)
{
LPC_I2C->DAT = data; 
  LPC_I2C->CONCLR = 0X28;//Clear Start Flag and SI Interrupt
  while(LPC_I2C->STAT!=status);  //Wait for the Status Byte
}
unsigned char I2C_Read(void)
{
  LPC_I2C->CONCLR = 0X28;
  while (LPC_I2C->STAT!=0x50);//Wait for Status Set - 0x50
  return(LPC_I2C->DAT);
}

[/syntax]

In function Read from RTCC (given below)

[syntax=c]unsigned char PCF8523_Read(unsigned char Address)
{
unsigned char temp;
I2C_Start();
UART_Write('1');
I2C_Write(PC8523_ADDRESS,0x18);
UART_Write('2');
I2C_Write(Address,0x28);
UART_Write('3');
I2C_Restart();
UART_Write('4');
I2C_Write(PC8523_ADDRESS+1,0x40);
UART_Write('5');
temp = I2C_Read();
UART_Write('6');
I2C_Stop();
UART_Write('7');
return temp;
}[/syntax]

[color=#f30]As i dont have debugger i checked the content of Status Bytes on UART, i found that for I2c_Start, the status byte contains 0x08 when sending rtcc address i am getting status = 0x18 and then after sending the address from where i have to read i am getting status = 0x28 which is correct.
Upto this point i am getting valid status responses, but after sending Repeated Start i am getting 0x28 each and every time continuously.
Can anyone please help me to solve this issue.[/color]
ラベル(1)
0 件の賞賛
返信
0 返答(返信)